NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I am designing a Matter/Zigbee Gateway using an STM32U5 as the host. My planned architecture includes:ST67W: Handling Wi-Fi and Thread (Matter over Wi-Fi/Thread).STM32WBA (or similar): Handling Zigbee (Matter Bridge logic).I have two specific q...
Hello Everyone,I'm quite new with this kind of coding.I'm editing two dual core projects written for Nucleo WL55JC1, Node2 and Node1. Node2 allready implements the reading from adc and now i have to implement into Node1. I would like that the "adc.c"...
Hi, I am working on proof of concept project with B-L4S51-IOT1A Discovery board with STM32 micro on board and many useful sensors for fast development, I am wishing to learn in the on board wireless sensors i.e. BlueNRG-M0 and Wifi. I want to load an...
Hi, I am prototyping a PINGPONG project on two NUCLEO STM32WL55JC1 with en.stm32cubewl-v1-3-0 software.I am checking the link at low Rssi values driving one board apart from the other.The parameters are below. I change OUTPUT POWER from 0 to 22dBm.I...
When generating code im getting two erros:In timer_if.c:in LoraMac.c: I've been trying to look for some answers but i couldn't really find something useful.If someone can help i'd really appreciate it.Regards.
Hello all,I am working with the STM32WB series and using a 32 MHz crystal for the HSE (specifically the Murata XRCGB32M000F1SBBR0 on my custom board).To verify correct operation, I measured the analog waveform on OSC_IN and OSC_OUT using a low-capaci...
I'm working with a NUCLEO-STM32WBA55 board and trying to build the BLE_p2pClient example project, but it fails with the error shown below:I../../System/Modules -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -...
HelloI was developing an application that uses BLE and low power mode. I was testing that on a custom board and when I measured the current consumption at STOP2_MODE, it was 1.7 mA.I expected that I had made a mistake. So I tried the low power exampl...
Hi, I am using STM32WBA55G-DK1, is it possible to use Audio In jack to send the input audio and at Out to receive the audio in a full duplex method. Thank you
Hi Community, I'm trying to build the BLE_TransparentMode example for the NUCLEO-WB05KZ, but I'm getting the following build error: region 'FLASH' overflowed by 93348 bytes Steps to reproduce: Open the BLE_TransparentMode example from the MX Examp...