STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 241 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4082 Views
  • 0 replies
  • 3 kudos

Resolved! Unable to build example project on NUCLEO-STM32WBA55

I'm working with a NUCLEO-STM32WBA55 board and trying to build the BLE_p2pClient example project, but it fails with the error shown below:I../../System/Modules -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -...

kclauah by Associate II
  • 436 Views
  • 1 replies
  • 0 kudos

Resolved! P-Nucleo-WB55 Low power examples

HelloI was developing an application that uses BLE and low power mode. I was testing that on a custom board and when I measured the current consumption at STOP2_MODE, it was 1.7 mA.I expected that I had made a mistake. So I tried the low power exampl...

STM32WB05KZ Build FLASH overflow

Hi Community, I'm trying to build the BLE_TransparentMode example for the NUCLEO-WB05KZ, but I'm getting the following build error: region 'FLASH' overflowed by 93348 bytes   Steps to reproduce: Open the BLE_TransparentMode example from the MX Examp...

Dadigno_0-1764347585364.png
Dadigno by Senior
  • 1137 Views
  • 8 replies
  • 0 kudos

Resolved! STM32WB Option Bytes read/write

Hi!In AN5289, on page 37, the sequence for writing to Flash memory is described, taking into account potential CPU2 access (semaphores Sem2, Sem6, and Sem7). What does the diagram for writing/reading option bytes look like? Is it the same?

Not able to write the values in the ble using custom

I am using the stm32wb55rev6 for my ble project.I created a new project based on the custom template provided by the ST. I am not able to print the messages on the terminal using the APP_DEBUG function.I am not able to send the data from the app to t...

TejasK by Associate III
  • 273 Views
  • 0 replies
  • 0 kudos

Resolved! Need M0+ recovery solution without reseting M4

Hi! We are developing a sensitive device using the STM32WB55, using in the M0+ the concurrent Thread+Ble binary (we use the concurrent because we'll need both Ble and Thread in the near future, althought the most important role is the Thread communic...

HAP Central start stream fail

Use example code BLE_Audio_HAP_Central to audio function. The Central may start the stream fail, though the BLE connect and GAP link returns are OK. and Once the stream start failed, the stream cannot be start forever, with the result "CAP Unicast St...

HuangFan by Associate II
  • 1552 Views
  • 16 replies
  • 0 kudos