NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I am trying to build an application on a STM32WLE5JBI6 that could work with confirmed downlinks. I thought that the LoRaMAC handled this but I could not find any mention of it in the documentation or in the code.As anyone already implemented it...
I want to capture the BLE air packet to parse the BLE connection event by using nRF52840 Dongle and wireshark, but I met a problem.I can capture the air packet normally when the slave device is advertising. But once the connection is established, I ...
Dear ST Community, Dear ST Team.For a evaluation of the chip i would like to try over LoRaWAN Communtication to set a LED on and off.Sadly on the tutorial program LoRaWAN_End_Node i get the ERROR: dev_nonce_too_small. The Problem is that on the Docu...
Hi, I am currently working on the NUCLEO WB55RG board on a project configured by CubeMX as BLE server. Everything is working correctly on this side. The problem is that I am using 4 boards as server and i would like to send a broadcast message (adver...
I'm working on inserting the STM32WB55 into stop mode2 via the tickless idle for the FreeRTOSI saw that the SDK has an example for it: in the BLE_HeartRateFreeRTOS example for the nocleo wb55 I went over the code of the SDK and there was one line whi...
Hello,I'm using a custom board which has STM32WB55 as the MCU. For the application, requires the MCU in sleep mode. The chosen sleep mode is STOP2. I referred the example project 'PWR_STOP2_RTC' which is available for the p-nucleo board and tried to ...
I am working with the STM32WB15 controller. I have implemented a few custom BLE characteristics and I want to be able to check the value of the characteristics on the server side (not from a read request from a client device). Is there a way to acces...
The STM32WL55 Nucleo board comes with the LoraWAN DevEUI, AppKey et al.I assume that this is not the case for STM32WL55CC mcu itself, right? And I have to work out how to write that into each device by myself.// Niclas
Hi,I am trying to commissioning NUCLEO-WB55RG Matter thread end device using chip-tool running on raspberry pi, It fails to commission.Reference Source Code used:Matter beta version for STM32 Github repo: github.com/stm32-hotspot/stm32wb-matter-devic...
I am using the stm32wb boards to learn OpenThread and develop a low power application to read some sensor data. My plan is to use a CoAP message to send the payload, and have been studying the THREAD_SED_Coap_Multicast example in an attempt to learn....