STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! stm32wb55 returns "unlikely error" when enabling notifications on a peripheral characteristic

I am developing a BLE product using the stm32wb and have it working as a peripheral/server.  I need to add the ability to work as a central also and am following the BLE_p2pRouteur example in STM32CubeWB/Projects/P-NUCLEO-WB55.Nucleo/Applications/BLE...

WB55 board is not appear on bluetooth list

I have a P-NUCLEO-WB55 board and i want to use it to communicate with my phone on ble. Fİrst of all, i decided to try an example to see if its works. I updated fus and then uploaded ble stack like the 11th video of STM32WB Getting Started Series Afte...

EPekg.1 by Associate
  • 1760 Views
  • 2 replies
  • 0 kudos

STM32WB55 USB audio driver support

I am currently working on a project that requires to implement USB audio in and out feature on STM32WB55 for connecting to PC. Is there any reference project that has this driver available? i tried working on FP-AUD-BVLINKWB1 but found that it is onl...

LoRa Option in STM32 Cube for bl072cz-lrwan1

Hi I am trying to create SubGHz project using STM32 Cube. When I choose the bl072cz-lrwan1 board, although this is an eval kit for LoRa, and has a PingPong example which uses LoRa and SubGHz, yet I can't find any option for SubGHz or LoRa in the midd...

sgabran_0-1688681447642.png
sgabran by Associate III
  • 2709 Views
  • 3 replies
  • 0 kudos

Resolved! RSSI on LoRa module

HiWe are using the the ST library calculates LoRa SNR and RSSI by capturing the readings in register "REG_LR_PKTRSSIVALUE" although there is another register called "REG_LR_RSSIVALUE".I failed to figure out the difference in contents of those 2 regis...

sgabran by Associate III
  • 3023 Views
  • 1 replies
  • 2 kudos

PingPong Example, failing to run GPIO ISR

Hi I have been trying to activate the callback function for the pushbutton in the SubGHz PingPong example, but with no luck. I am using the BSP_PB_Init() to configure the pushbutton: void BSP_PB_Init(Button_TypeDef Button, ButtonMode_TypeDef ButtonMo...

sgabran by Associate III
  • 4137 Views
  • 6 replies
  • 1 kudos