NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
1. I have been using STM SDK v1.3.0 with lorawan version 1.0.4.2. I want to force rejoin whenever no NVM context data is restored and rejoin using previous information whenever NVM context is restored.3. But when I try to force rejoin, I get the foll...
Hello I need help to update my fus in stm32wb10ccu5. If there is any expert available from Stm please reply.
After going through AN5270, I have a few questions.I realize that there can be up tp 2 connection to slave.Can I read the current list of connected devices ( not yet paired) from the stack via an HCI/ACI command?As for LIMITED_DISCOVERY command can T...
Hello all,Working on communication between two STM32WB55 boards , one configured as client , and one as server.When trying to write a characteristic I get a bad parameter error, but when I use the write characteristic long command it works fine.Writi...
I am writing an application that utilizes the BLE functionality of the STM32WB to scan for BLE beacons. In all support materials I've found that show how to exploit the BLE functionality of the STM32WB your code must be coupled to the sequencer and S...
Hello,I'm pretty new in working with STM32WB-Chips and trying to implement a BLE-Application.I am using a STM32WB55 Chip and for initial steps I created a project using Cube IDE and a Custom Template according to ST's "Getting Started" - Series on Yo...
Hi,I have attached code for .ino .cpp .h has changed to txt file attached here, please verify my code i get error server for erase function failure. and some time not working properly please assist us. please say how to solve this issue. my error was...
Hello! I am trying to get Wireless Firmware Upgrade to work on an STM32WB5MMG.I have managed to get it working with the example project in the STM32WB repository.This is FUS information: When I flash this project onto the device with STM32CubeIDE, I ...
Hi,I am trying to transfer 2k bytes data every a while (20s for example) from BlueNRG-LP to my computer with one connection event. the 2KB data is divided into 5 chunks (data packets), which means 5 data packets contain a complete data set. After I ...
Board: STM32WB55Software: STM32CubeIDEBackground: I am experimenting with a Custom Bootloader to enable USB and BLE updates to my firmware. I'm getting the IDE to export .bin and .hex files on build, so I can pass my main application into the bootloa...