STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 235 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4077 Views
  • 0 replies
  • 3 kudos

ERROR : ERR_THREAD_CHECK_WIRELESS

get an error when debugging the example application:STM32Cube_FW_WB_V1.17.2/Projects/P-NUCLEO-WB55.Nucleo/Applications/Thread/Thread_Coap_Genericerror:[M4 APPLICATION] **********************************************************[M4 APPLICATION] WIRELES...

jfc54 by Associate
  • 1425 Views
  • 1 replies
  • 0 kudos

GSM AT Command response

Hi I am sending a AT command through USART2 -char CGSN[] = "AT+CGSN\r\n";HAL_UART_Transmit(&huart2,(uint8_t *)CGSN, sizeof(CGSN),100);HAL_Delay(500);  HAL_UART_Receive_IT(&huart2,(uint8_t *)&ch,1);I am receiving ch in callback and storing each byte ...

KPeri by Associate II
  • 2482 Views
  • 3 replies
  • 0 kudos

LoRaWAN_End_Node (Uplinks - STM32WL55JC)

Hi,I am developing a LoRaWAN project using the ST code (LoRaWAN_End_Node). int main(void){HAL_Init();SystemClock_Config();MX_LoRaWAN_Init();MX_GPIO_Init();MX_I2C1_Init();MX_TIM16_Init();HAL_TIM_Base_Start_IT(&htim16);while (1){MX_LoRaWAN_Process();}I...

STM32WB BLE performance with sequencer, android

We're working with the STM32WB developer board and we've encountered "slow BLE writes" with android.While trying to make our BLE writes faster, we determined that if we remove the "GATT_NOTIFY_WRITE_REQ_AND_WAIT_FOR_APPL_RESP | GATT_NOTIFY_READ_REQ_A...

FwPro by Associate
  • 1803 Views
  • 2 replies
  • 0 kudos

WB35 BLE application not working

Here at the university we have some projects using STM32WB for BLE applications, but we only have succeeded after messing around with teh BLE_CUSTOM example and overwriting some info into the ioc via notepad (it was used to be able to change the file...

BLE - Single peripheral to multiple central connection

Using the NUCLEO board with STM32WB.Device is currently configured as server to act as a peripheral. (one of the examples)I am interested in connecting it to multiple central.Is it possible?Any example will be great.

DS.4 by Senior II
  • 1601 Views
  • 2 replies
  • 1 kudos