To use a clock to drive the RF unit of the STM32WB55, here are 2 options in the BLE_p2pServer demo code, LSE and HSE divided by 1024,I want to know if it is available to use LSI or HSI as the clock source of RF unit in it, thank you.
About reading tags via USB UART by ST25RU3993 without ST25RU3993 Reader Suite GUI.To initial and start reading tags automatically after plugged in and print them on serial terminal (ex: Tera Term) via USB UART (not the UART LOG pin) by ST25RU3993 wit...
Dear Nick,I've successfully booted the EVB by set DTR to low and toggle RTS low - high and enabled the device mode, thank you so much for help me to solved this issue. But here is an error occurred, as the following picture, the EVB crashed when it...
Dear Nick,I have enable the STUHFL_DEVICE_MODE in main.c of the firmware and flashed into the ST25RU3993 HPEV board, but it still need to click "Connect Reader" on the ST25RU3993 Reader Suite GUI and thenstart working, if I launch Tera Term and conn...