User Activity

I have been trying to have the STM32WB55 save the OpenThread network information after joining the network, so that it can automatically join it upon power cycle. After joining the network through the commissioning process, I call SHCI_C2_FLASH_Store...
I have been using the STM32WB55 Nucleo board successfully to run a CoAP server on OpenThread.I have designed a custom board which is very similar to the Nucleo board (same microcontroller).I successfully updated the FUS firmware following the Release...
From the STM32CubeWB firmware package, there is a Thread_RCP project. However, there doesn't seem to be any documentation for it (it is not even mentioned in AN5289). The only hint is the readme.txt file which says: "This application is used to demon...
Hi there,I am using a 800x480 display that does not have square pixels. Therefore, my custom containers are always "stretched" along the y-axis. This is not a problem for static images in my container, since I can scale the image before on the PC sid...
Hello,I have made a custom board based on the STM32F746. I am using a touch panel which uses the FT5436. My question is: are the FT5336 drivers provided by with the STM32F746 discovery board drivers compatible with the FT5436? I cannot make it work. ...
Kudos from