STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! BLE (UTIL_SEQ_SetTask) and EXTI conflict?

I made a PCB board with STM32WB5MMG, which receives the data of max30112 through external falling edge interrupt and sends it through BLE notify. However, once I add the execution task UTIL_SEQ_SetTask(1<<CFG_TASK_SPO2_EVT_ID,CFG_SCH_PRIO_0); in HAL_...

Lep_0-1696575523900.png
Lep by Senior
  • 4141 Views
  • 4 replies
  • 0 kudos

BLE mesh and FLASH access problem

Hello,I am trying to develop app based on BLE_MeshLightingProvisioner example. From the readme file, I know that the node can be self provisioned and configured when the ENABLE_PROVISIONER_FEATURE is defined. This is a great feature and I want to use...

0693W000000WE0xQAG.jpg 0693W000000WEC5QAO.png
lukasz2 by Associate III
  • 4221 Views
  • 8 replies
  • 0 kudos

COMP 2 INPM some Pins are not working as expected

Hi,I am using comp2 for our project ( STM32WB5MM )were we use INP Plus and INP Min Pins for the comperator,for INP plus I Use the PB4 and For INP Min i want to use the Pin PB3 or PB7 but unfortunately I am not getting interrupt at disered voltage, bu...

VJani.11 by Associate
  • 1381 Views
  • 1 replies
  • 0 kudos

STM32WB55 interrupt blocking BLE

Hi everyone,I am actually working on a project based on a custom STM32WB55 platform with a LIS2DTW12 (accelerometer) embedded.I am having an issue with a code based on the BLE_p2pserver example code. I am using the LIS2DTW12 dataready interruption as...

RKalm by Associate
  • 2339 Views
  • 2 replies
  • 0 kudos

STEVAL-STWINBX1 and LoRa

Hello, Could you please tell me what equipment I need to buy to transmit data from STEVAL-STWINBX1 via the LoraWan protocol?Thank you in advance for your answer