NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have just downloaded the reference board from the STM32WB55: STM32WB55RG - Ultra-low-power dual core Arm Cortex-M4 MCU 64 MHz, Cortex-M0+ 32 MHz with 1 Mbyte of Flash memory, Bluetooth LE 5.4, 802.15.4, Zigbee, Thread, Matter, USB, LCD, AES-256 - S...
I’m using a STM32WB5MMGHx module on a battery powered device. When the module loses power due to low battery or the battery being removed it does not advertise after regaining adequate power. Only after restarting or reflashing the wireless stack do...
Hello, how can I call a full reset of the CPU2/BLE stack (as if the device were powered up)?I'm resetting CPU1, which then restarts the CPU2/BLE stack from some other code. But this causes some corruption with BLE notifications.
Hi everyone, I try to debug CM0+ core (using GDB server) application LoRaWAN in SBSFU dual core project. If I only run the debugger on CM4, the program will start and run normally. But when I try to debug CM0+, it will not run and my program failed.I...
STM32WL lorawan middleware use a RTC subsecond underflow interrupt update tick instead systick,but the subsecond underflow interrupt never entered.It seems interrupt not enabled, so I manually enable RTC subsecond underflow interrupt but the handler ...
Hello,What I have done:- Following instructions from AN5185 document.- Using STM32CubeProgrammer v2.14.0- NUCLEO-WB15CC powered on- With STM32CubeProgrammer :- ST-Link configurationST-Link upgrade (v3.12.3)Update to firmware V2J42M27- ST-Link Connect...
Good morning,I am creating an application that would require the use of several stm32wl55.The idea is to have one microcontroller configured as a LoraWan EndNode communicating with TTN and a set of Slaves communicating via subghz (which will be slave...
In the STM32WB Workshop video I can understand how to send data and control the LED but how to read data is not explained. I want to read data from STM32WB BLE. Can you someone help me in regards to this?
Hi,I'm looking for the max size of SRAM allocated for the GATT database for the STM32WB series.I've found the informations for WB55 and WB15 but I can't find the information for WB10/30/35/50/. Does anyone know these values or how it can be calculate...
Hey guys. I'm trying to collect the sigfox credentials through the website https://my.st.com/sfxp and once the download is done,the file is corrupted and I can't extract it.How can I solve this problem?