2023-04-11 11:52 PM
In my opinion there are two bugs HAL_RTC_SetTime(..) (p. 776) and HAL_RTC_GetTime(..) (p. 881).
/* Check Binary mode ((32-bit free-running counter) */
if (READ_BIT(RTC->ICSR, RTC_ICSR_BIN) != RTC_BINARY_ONLY)
should be RTC_BINARY_ONLY instead of RTC_BINARY_NONE.
Solved! Go to Solution.
2023-04-12 4:08 AM
Hello @ANalb.1 and welcome to the Community :)
The latest version of STM32CubeWL v1.3.0 contains this line:
/* Check Binary mode ((32-bit free-running counter) */
if (READ_BIT(RTC->ICSR, RTC_ICSR_BIN) != RTC_BINARY_ONLY)Imen
2023-04-12 4:08 AM
Hello @ANalb.1 and welcome to the Community :)
The latest version of STM32CubeWL v1.3.0 contains this line:
/* Check Binary mode ((32-bit free-running counter) */
if (READ_BIT(RTC->ICSR, RTC_ICSR_BIN) != RTC_BINARY_ONLY)Imen
2023-04-13 2:21 AM
Sorry
2023-04-13 2:47 AM
If you are satisfied of my answer, please mark it as "Best" by choosing Select as Best, so that this thread will be marked as solved.
Imen