NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, I just came accross the STM32WL series and I was wondering if I can implement a different modulation other than the ones included (FSK, PSK). I need to acquire an analog signal, convert it to digital and then modulate it with a frequency modul...
Good Morning,I am working with an engineer that needs to asses the current based on the states of the STM32WB. Is the simplest approach to use the Nucleo Board with the part and then, reviewing the schematic, place a current meter in line with the j...
Dear St,I'm developing a cluster with a client and server, where I have a client to write on the cluster of the server. I can write with the function ZbZclWriteReq() on the server, but I'm not always successful. When I do the first write, I have succ...
Hello, I'm using the client/server example with two Nucleo-WB55 kit, it works without issue.Now I'm working with my own board:Client : STM32WB5MM moduleServer: the same nucleo-WB55 as above At starting, the client scans and detects the server(with th...
Hello Developers, In our product, we currently have a RAK3172 module interfaced with STM32L4 controller. I am able to use both LoRa P2P and LoRaWAN communication using the AT command sent to the RAK chipset from host, through UART interface. Now i wo...
I do everything as decribled here:-stm32u5 program with ble at client code-on stm32wb I update fus, stack and program BLE_AT_Server_reference.hex from STM32Cube_FW_WB_V1.17.0When i try run app @teraterm i see:Start of the STM32WB5M module AT examp...
Hi team, Warm GreetingsI am using STM32WB55RG6VTR controller in our battery operated product development. We are enabling the sleep mode in the controller to test the current which is around 10mA but it is supposed to be around 40uA if all peripheral...
Hi all,I have a setup where many devices need to to respond to a message on 868MHz from a sender. At the moment I am using random delay to space the responses but I will like to use the RadioIsChannelFree() function.Do anyone use this function? Is it...
Hello community,Currently, I have Lorawan gateway: p-nucleo-LRWAN1 and Lorawan node: B-L072Z LRWAN1.I'm looking forward to suggestions from you, which company gateway and node will be better than this current gateway and node. with current devices, I...
I encounter the following error when connecting STM32WB15 to ST-Link V2.Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authenticationonly VDD,GND, and SWIO and SWCLK pins connected..p...