cancel
Showing results for 
Search instead for 
Did you mean: 

What can prevent entering STOP mode? (STM32WB)

OliM
Senior II

After some activity using BLE in the background and UART as well as some EXTI on application side, the consumption jumps from 2,4µA to 4mA, so obviously I have a wakelock. If I hotplug to the system afterwards, I can see in PWR_EXTSCR that Stop mode is no longer actually reached (C1STOPF is not set). But checking ISPR I can not see any pending ISRS (the one after Stop is the LPTIM of my OS).

What else can prevent the CPU from entering stop? Which registers should I check?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0