Currently we are using STM32F4 & STM32H7 controller with inbuilt ethernet. We are looking to add a profinet interface in our device without using additional external hardware.Please can you share references or documents how can we integrate Profinet ...
Hello,Does ST plan to support Matter over WIFI? Is there any EVK which is available to test Matter over WIFI. If yes, please provide us the details of EVK as well as source code.Best Regards,Pavan
Hello,I am trying to commissioning NUCLEO-WB55RG Matter thread end device. It fails to commission and connect.Reference Source Code used:Matter beta version for STM32 Github repo: github.com/stm32-hotspot/stm32wb-matter-device-over-thread Setup:1. M...
Hello Remy,It works with the Chiptool Application provided with the package.Can you please provide us the source code of Android CHIPTool.Best Regards,Pavan