NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,I have seen that the new STM32WL33 have support for 4-FSK, high receive sensitivity and wake-up receiver LPAWUR, which is beneficial for both high-data-rate and long-range applications. However, LoRa support is reserved for STM32WL55 and STM32WLE5...
I doubt if the ST-link has some setting problems?Model:P-NUCLEO-WB55 PNWB55$CU301:09:41 : Warning: FUS_STATE_IMG_NOT_FOUND, Flash already empty !01:09:42 : Firmware delete Success01:09:42 : Download Stack/FUS image at address 0x80EC000 ...0...
Hey folks,I'm having issues with the RTC's calendar function while using BLE. I would like to timestamp recorded data using the calendar function of the RTC and then transmit that data over Bluetooth. However, when I enable the Bluetooth middleware i...
assert_failed() is being called inside BleStack_Init() with USE_FULL_ASSERT defined. By default, Stm32CubeMx does not define USE_FULL_ASSERT so assert_failed() would have never been called. Either way, BleStack_Init() returns zero causing APP_BLE_I...
Hello!I'm using the STM32WL55CCU6 in a design and have a question:TCXO: I'm using a TCXO connected according to the datasheet. If I select TCXO in CubeIDE I have to use PB01 as TCXO-VDD. My plan was to use PB01 as GPIO. Is that possible? How? -> If i...
Hi ST Team, I have found this post here, which explains how to power the Nucleo WB55RG board with an external power source. https://community.st.com/t5/power-management/powering-nucleo-wb55-externally/m-p/632719#M10752Now I have a followup question: ...
Hello,I have been following the tutorial STM32CubeMX Application Conception for making a custom BLE server with my P-Nucleo-WB55. I am using version 6.9.2 of STM32CubeMX. Everything works until section 7, where server notifications and write manageme...
Hi, am using the STM32WB55 Nucleo board. My problem is, currently Iseem not to have a CPU2 wireless stack loaded and I fail to load filestm32wb5x_BLE_Stack_full_fw.bin loaded into the Flash. I am using theSTM32CubeProgrammer V2.12.0. When selecting o...
Hi,I'm working on STM32WB10CC with 320KB of flash memory.I'm using the full ble stack 1.14.1 (stm32wb1x_BLE_Stack_full_fw.bin) which has a size of 148KB.In the release note it's written you have to put it at this address 0x08021000.If I'm doing the m...
Hi, I'm currently involved in implementing the transmission of variable-length data within Zigbee clusters. While I've successfully managed operations related to the String data type, I'm encountering challenges with the struct data type. I would ap...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.