STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 223 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Resolved! Pulse sensor and input voltage

Good morning,I am building a system with stm32 wl55jc1 to count water flow with a pulse flow meter.So I created two internal clocks in stm32 one to create a time window and the other that counts each pulse received from the sensor. At the trigger of ...

IngSerio by Associate III
  • 2303 Views
  • 2 replies
  • 1 kudos

SPIRIT library and Sub_GHZ lib compatibilty

Hi A previous version of a product used STM32G071x8/xB in conjunction with external radio transceiver (SPSGRF-915). The team has used SPIRIT middle ware for radio functions. A newer version has migrated to STM32WLE5/E4xx which has inbuilt radio and I...

pavitrar by Associate
  • 1702 Views
  • 2 replies
  • 0 kudos

STM32WB55 ACI_GATT_NOTIFICATION_COMPLETE_EVENT never fired

Hi,I am using aSTM32WB55Wireless Firmware version 1.17.2Wireless Firmware build 1FUS version 1.2.0As described by AN5270 2.5.6. an ACI_GATT_UPDATE_CHAR_VALUE must fire an ACI_GATT_NOTIFICATION_COMPLETE_EVENT if the characteristic was created with GAT...

Resolved! STM32WB5MM-DK unable to connect over Matter

I am attempting to use the https://github.com/stm32-hotspot/stm32wb-matter-device-over-thread/ repo to connect a STM32WB5MMG-DK to an Amazon Alexa acting as a border router, using the Alexa app. The device always fails to connect, outputting the seri...

RHeyse by Associate
  • 5683 Views
  • 3 replies
  • 0 kudos

STM32WB55 BLE connection issues at higher temperature.

Hello!  We are a bit stumped here.  We have a product that we are testing at 65C and it seems that the bluetooth connection keeps dropping at this temperature (Connection timeouts).  We are running from a 32K LSE and 32M HSE crystals.  All our parts ...

BStic.2 by Senior
  • 2158 Views
  • 3 replies
  • 0 kudos

Why STM32WL Alarm always wakeup advance 1 second

I use STM32WL RTC Alarm as low power mode timer for achieve ms level accrancy and any duration sleep. System will convert sleep time to Alarm time before enter low power mode. I have tested different  sleep time, verified convertion result is correct...

st_post_1.png
SimonLaw by Associate
  • 2104 Views
  • 2 replies
  • 2 kudos