STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 248 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4084 Views
  • 0 replies
  • 3 kudos

STM32 WL55JC1 LoRaWAN Class C not working!

Dear community, In the attachments, I am sending You two screenshots, one from the LoRa WAN Network server and the other one from the STM32CubeIDE. We are using two of Your dev boards, one as the LoRa WAN gateway (Nucleo F746ZG) and the other one as ...

fainlaip by Associate II
  • 2714 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WL33 with LoRa

Hi,I have seen that the new STM32WL33 have support for 4-FSK, high receive sensitivity and wake-up receiver LPAWUR, which is beneficial for both high-data-rate and long-range applications. However, LoRa support is reserved for STM32WL55 and STM32WLE5...

MB1355C firmware upgrade, FUS_STATE_IMG_NOT_AUTHENTIC

I doubt if the ST-link has some setting problems?Model:P-NUCLEO-WB55           PNWB55$CU301:09:41 : Warning: FUS_STATE_IMG_NOT_FOUND, Flash already empty !01:09:42 : Firmware delete Success01:09:42 : Download Stack/FUS image at address 0x80EC000 ...0...

Baochun by Associate
  • 1565 Views
  • 1 replies
  • 0 kudos

Resolved! Can the RTC's calendar function be used alongside BLE?

Hey folks,I'm having issues with the RTC's calendar function while using BLE. I would like to timestamp recorded data using the calendar function of the RTC and then transmit that data over Bluetooth. However, when I enable the Bluetooth middleware i...

0693W000004KVwMQAW.png
burn_ by Associate III
  • 4183 Views
  • 5 replies
  • 0 kudos

Resolved! STM32WL55 TCXO-PB01

Hello!I'm using the STM32WL55CCU6 in a design and have a question:TCXO: I'm using a TCXO connected according to the datasheet. If I select TCXO in CubeIDE I have to use PB01 as TCXO-VDD. My plan was to use PB01 as GPIO. Is that possible? How? -> If i...

robha by Associate
  • 1933 Views
  • 1 replies
  • 0 kudos

Nucleo WB55rg powering CPU only

Hi ST Team, I have found this post here, which explains how to power the Nucleo WB55RG board with an external power source. https://community.st.com/t5/power-management/powering-nucleo-wb55-externally/m-p/632719#M10752Now I have a followup question: ...

whati001 by Associate II
  • 2210 Views
  • 2 replies
  • 0 kudos

Resolved! BLE Custom Application Issues

Hello,I have been following the tutorial STM32CubeMX Application Conception for making a custom BLE server with my P-Nucleo-WB55. I am using version 6.9.2 of STM32CubeMX. Everything works until section 7, where server notifications and write manageme...

RCM1_1-1709500350335.png
RCM1 by Associate II
  • 3154 Views
  • 4 replies
  • 1 kudos

Cannot load Wireless firmware into STM32WB55 Nucleo board

Hi, am using the STM32WB55 Nucleo board. My problem is, currently Iseem not to have a CPU2 wireless stack loaded and I fail to load filestm32wb5x_BLE_Stack_full_fw.bin loaded into the Flash. I am using theSTM32CubeProgrammer V2.12.0. When selecting o...

zabel by Associate III
  • 6561 Views
  • 12 replies
  • 0 kudos

Resolved! STM32WB10 flash memory distribution

Hi,I'm working on STM32WB10CC with 320KB of flash memory.I'm using the full ble stack 1.14.1 (stm32wb1x_BLE_Stack_full_fw.bin) which has a size of 148KB.In the release note it's written you have to put it at this address 0x08021000.If I'm doing the m...

Coco_3-1709658039480.png Coco_1-1709657878769.png
Coco by Associate III
  • 2770 Views
  • 4 replies
  • 1 kudos