STM32WB missing HCI_LE_CONNECTION_UPDATE_COMPLETE _EVENT
I have been testing with two STM32WB boards, one as central and the other as peripheral. I read in the document "Building wireless applications with STM32WB Series microcontrollers" (newest member cannot add links so I could only paste the title of the document) in section 6.9 that the master can initiate `aci_gap_start_connection_update()` to update the connection parameters, and the end of procedure will be indicated with an HCI_LE_CONNECTION_UPDATE_COMPLETE
_EVENT.
However, I didn't seem to be getting any event on both central and peripheral, even though I could sense the update taking effect and the update was actually completed.
As I'm new to bluetooth, I don't know what the possible reason for missing events could be. I don't have problems with other events such as the completion of general discovery or connection establishment. Connection updating is the only one I'm having an issue with. Please help! Thanks!
EDIT: After some more testing, I noticed only when the update caused change to the connection interval would there be an event. But in my case I only want to update the CE_length and I don't know why there is no event for this.