Skip to main content
Martin.Sergio
Associate III
February 23, 2021
Question

Recommended NT2016SF-32M-END5875A for STM32WL design

  • February 23, 2021
  • 16 replies
  • 7657 views

We design a new product where we use STM32WL microcontroller and in the datasheet ST is recommended to use NT2016SF-32M-END5875A

manufactured by NDK but we dont found it to buy.

Can you provide some distributors where we can buy this TCXO?

Can you provide other alternative TCXO to NT2016SF-32M-END5875A?

Thanks a lot and best regards

16 replies

DedMoroz
Visitor II
February 23, 2021

Did consider to use a regular 32Mhz HSE?

Martin.Sergio
Associate III
February 24, 2021

No, we have not considered using a a regular 32Mhz HSE because temperature variations will be constant, not only because the equipment will be outdoors, but also because the RF circuit produces temperature increases.

Hamilton DC
Visitor II
February 24, 2021

Note that there is a global shortage of TCXO due to a fire at an Asahi Kasei Microdevices (AKM) factory in Japan. 

DedMoroz
Visitor II
February 24, 2021

We designed a prototype with WLE5 without TCXO. The RF part not tuned at all and we got only 20m distance inside the building with 4db output, but I look forward for a better results. We also consider to change SUBGHZ_HSEOUTTRIMR values dynamically based on the outside temperature to keep the crystal tuned.

Hamilton DC
Visitor II
February 25, 2021

If you're designing LoRa applications, then the recommendation is:

For high power applications (RFO_HP), use a TCXO instead of XO (crystal) as HSE clock source due to frequency drift issues.

For low power applications (RFO_LP), you can use an XO as HSE clock source with a thermal barrier on the PCB (no metal around the XO to reduce thermal conduction).

Aagra.11
Associate
April 19, 2021

Hi Hamilton,

thanks for your reply. Can you help me understand how much drift can be there if i used normal crystal? also i want to understand the maximum allowed PPM for the crystal in tolerance and stability for STM32WL. I have gone through the AN2867 , but it does not give me these questions answers.

My application will be outdoor and 22DBM module with 865MHz (Indian) frequency band.

kindly help.

regards

Ankush Agrawal

Hamilton DC
Visitor II
August 23, 2021

Hi @Aagra.1​ ,

In the datasheet, Search for FERR_L, HSE32 crystal requirements, HSE32 TCXO regulator characteristics for more information. Concerning the question about frequency drift, please, see my answer below. Do not confuse frequency drift with FERR_L. It's not the same thing. The frequency drift occurs during a packet transmission when the frequency of Tx drifts due to heat (from the device) propagation reaching the crystal. The heat generation is related to the RF output power.

FZ_
Visitor II
March 27, 2021

We have encounter the same problem. Could someone from ST, recommend ano other VCTXCO to replace NT2016SF-32M-END5875A which is used in the EVB Nucleo. In our project as well, the temperature variation is very important. Using a regular 32MHz HSE, is not the best option.

Could this product be used as an alternative:

https://www.iqdfrequencyproducts.com/products/details/iqxt-205-2-1-01.pdf

Thanks.

phoenixSun35
Associate
March 31, 2021

@DedMoroz​ Try without XTAL caps. I have suffered for one week to recognise it.

Senior
January 25, 2022

Dear @Hamilton DC​ ,

since the NT2016SF-32M-END5875A cannot be found from distributors (even the datasheet is not available).

Could you provide the specs of such device (pin capacitance, frequency stability, power supply, etc...)

or at least provide an alternative component?

Even the application note AN5042 doesn't give information either the datasheet of the STM32WL55XX (pag. 99): https://www.st.com/resource/en/datasheet/stm32wl55jc.pdf

Here, only the requirements for the HSE are present but not for the VCTXCO.

Can you give this information for making a custom board?

For example, could the TXEABDSANF-32.000000 be used in place of the NT2016SF-32M-END5875A?

Here the datasheet: https://www.taitien.com/wp-content/uploads/2015/12/XO-0076_TX.pdf

Thanks a lot

AElgh
Associate III
February 5, 2024

Any update on this topic?

Visitor II
October 17, 2025

Any update for NT2016SF-32M-END5875A ?