NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am trying to detect my stm32wba52cg bare chip with my developed custom PCB board with onboard stlink as external programmer from a discoveryboard but its showing this msg-Can not connect to target!Please select "Connect Under Reset" mode from Targe...
Hi together,I am working with the STM32WB55 and connecting it with different configurations to Homeassistant via Zigbee2mqtt.The Zigbee2mqtt auto generates a config file with the available endpoints etc., that looks like this:const definition = { ...
Hi ST Experts, We have a BLE project based on the STM32L476 and HM11 BLE and we are looking to minimize the component count and shrink the board size. We want to replace the STM32L476 with a BLE and MCU single chip solution and we are considering the...
Dear Sir, I use wl33 mcu with rtos, but when I set to stop mode, It didn't success. Is there a freertos examle? If I want to sleep with freertos in IDLE task , how can I achieve?
Hi, I'm currently just for learning experience trying to learn about Zigbee and how it works through IPCC. This boils down to a program that I wrote that tries to setup the Zigbee stack.I've OnOff_Server_Coord example as a guidance on how it should b...
Hi,I have many routers for sending data to the coordinator. I want to use table routing. How can I implement this? And how does table routing work? What happens behind the scenes?Best Regards,
Hi allIm using Nucleo WBA52CG development board with STM32Cube FW_WBA V1.4.0After generating code for BLE using STM32_WPAN i get error ble_wrap.c: No such file or directoryAny help?
When configuring the LCO output on an STM32WB05TZ with STM32CubeIDE 1.16.0 using STM32Cube FW_WB0 V1.0.0, the Generated code is missing the GPIO "Alternate" parameter, as a consequence, the output does not appear in the pin.Below is the fix that work...
Hello Community,Greetings of the day.I'm using the Nucleo WB55RG board. I'm trying to initialize and connect the wb55rg BLE with my mobile app.So, I'm following the stm32wb getting started video series, video part-12b. (video link - https://youtu.be/...
Colleagues.The STM32Cube_FW_WB_V1.20.0 library for STM32Cube_MX version 6.12 allows me to create DMA2 channels for B-WB1M-WPAN1. However, the startup_stm32wb1mxx_cm4.s and stm32wb1mxx.h files do not contain DMA2 interrupt vectors. Error[Pe020]: ident...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.