Hi,
I work with stm32wle5 where AT commands are received from LPUART. This interface is setup for 9600 bps / 8N1 and its baudrate clock is derived from LSE (32768Hz) clock. The chip is wake up by incoming characters.
I observe that transmitted bits h...
Hi,Binaries provided in S2-LP Development Kit v.1.3.3 (en.stsw-s2lp-dk_firmware) are newest than sources provided in that package:Binaries version: 2.3.3Source code: 2.3.0Please provide the sources that were build to that binaries (this ask is direct...
Hi,I am trying to create some first GUI application for STM32F429I-DISCOVERY just to learn TouchGFX. Unfortunately, when I start GenerateCode in TouchGFX Designer following error appears:Generate Code Generate Done Generate Assets make -f sim...
Hi,I use my device for continuous scanning. The scanning is started by calling:aci_gap_start_general_discovery_proc(
2000 /*LE_Scan_Interval = 1.25 s */,
1800 /*LE_Scan_Window = 1.125 s */,
0x00 /*=use public dev ad...
Hi,"I can imagine a "phase-accumulator", to which 256 is added every flck tick. (Or perhaps better, 128 every rising and 128 every falling fclk edge; I don't know which)."Thank you, it may be done this way. I need a confirmation from ST. "Changing ba...
Hi,yes I read it.Everything is set properly, but errors appears. More serious is that the chip stops receiving data.Transmitted characters comes from another stm32 that uses LPUART (clocked from LSE).There is jitter in bits as well.Regards,Piotr Roma...
Hi Winfred,thank you for the comprehensive migration guide. I found there some new information.In general, I know the step needed for porting, but this is some extra work to be done.It would be nice to have a version of project for IDE that is owned ...