STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32WB55CGU7 BLE client configuration

Hello Team,     I am Priya from Illuminen Technologies working as an Embedded Software developer. We are working with STM32WB55CGU7 BLE controller for our application. We need to use this module as client and server with two individual modules. And a...

PRIYA_En_0-1737457965095.png PRIYA_En_2-1737458151318.png PRIYA_En_1-1737458102989.png
PRIYA_En by Associate
  • 1000 Views
  • 1 replies
  • 0 kudos

LoraWAN Context Manager

Hi everyoneI having  issues trying to use "CONTEXT_MANAGEMENT_ENABLED " option in LoraWAN examples . I couldn't find "nvmm.h" library. Where can I find it ?.Is this feature fully functional ? Do you have any examples or is it just activate the "defin...

JesusAVC by Associate II
  • 1826 Views
  • 4 replies
  • 0 kudos

Resolved! A question about the STM32WB55RG dev board

I've been doing some BLE development using STM32WB55RG mounted on Nucleo-68 board. Our end product is very space constrained & doesn't need all the headers, switches etc that the board provides.So I took a loser look at what we could save space by re...

Resolved! STM32WB55RG not showing when using STM BLE Toolbox

STM32WB55RG not showing when using STM BLE Toolbox. In fact NO Bluetooth devices are showing at all.When I use the LightBlue app or scan using the Bleak Python library on my laptop, all discoverable devices are showing, including the STM32WB55RG with...

Zigbee end device not waking up in sleep mode

Hey,I have two problems regarding custom clusters and sleepy end devices. I want to create an SED that periodically sends custom long string messages (via attribute reporting) to a coordinator.1.Question:For this I implemented a custom cluster with a...

Name by Associate III
  • 9528 Views
  • 20 replies
  • 0 kudos

Adding client services stm32wb1

Hi,I am currently getting familiar with the STM32WB15 microcontrollers using two WB1M-WPAN1 boards.On the server/peripheral side, everything works correctly (the declaration of services and characteristics in the .ioc file is very convenient), and I ...

MorganLR by Associate II
  • 2267 Views
  • 6 replies
  • 0 kudos