STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

Resolved! Unable to enable BLE on the STM32WB07CCVX in STM32CUBEMX

I'm unable to enable STM32_BLE in "sofware and middleware" on the STM32WB07CCVX  in STM32CUBEMX as it's greyed out. Also, "RADIO" is greyed out too. Are there any guides on how I can set up BLE in STM32CUBEMX or does anyone know why these options are...

JTurn.2 by Senior
  • 1243 Views
  • 2 replies
  • 1 kudos

Resolved! Unable to build example projects NUCLEO-WB05KZ

STM32CubeIDEVersion: 1.12.1Build: 16088_20230420_1057 (UTC)I am trying to use one of the examples from the STM32Cube_FW_WB0_V1.1.0 package, but I am unable to build any of them.After importing the project into STM32CubeIDE (I have tried BLE_Beacon an...

Cattura.PNG

Resolved! STM32WL5MOC bootloader mode

Hello,  I'm looking for advices to place the module STM32WL5MOC in bootloader mode from different methods : Through BOOT0 and NRST but I can not find the communication interface that I can communicate with (for example UART) this specific mcu in the ...

User2501 by Associate II
  • 1160 Views
  • 1 replies
  • 0 kudos

Resolved! EEPROM Emulated Timing (x-cube-eeprom)

I am running a bluetooth application using freeRTOS on a Nucleo-WB55 (STM32WB55RG). I am in the process of implementing Emulated EEPROM (X-Cube-EEPROM) to store som data. After implementing eeprom emulated in a ble_heartrate_freertos example I have h...

Nikolaj_TL_0-1737036301238.png Nikolaj_TL_1-1737036338860.png Nikolaj_TL_2-1737036512206.png Nikolaj_TL_0-1737037736034.png

Cube MX Bug report for Zigbee Projects

Hi, I want to report two code generation bugs in Cube MX for Zigbee projects:Color Control: having a color control functionality requires to fill out capabilities, such as XY or HS color settings. Those capabilites are not saved when regenerating the...

vh789 by Associate III
  • 2927 Views
  • 7 replies
  • 0 kudos

Resolved! STM32WB55CC BLE stack not initializing

Hello,I'm trying to implement BLE functionality on a custom board equipped with an STM32WB55CC using CubeMX.I managed to successfully (or so I think, the option bytes look good) install the BLE stack binary, but the device is not advertising. I mana...

Resolved! STM32WLE5 Module JOIN FAILED

Hi,I'm doing tests based on the LoRaWAN_AT_Slave. One of the modules often appears tMAC txTimeOut, resulting in JOIN FAILED. Same firmware downloaded, but some devices are working, is there any doubt? Is it a hardware problem? [14:47:35.933]发→◇AT+JOI...

ethan2 by Associate II
  • 1303 Views
  • 2 replies
  • 0 kudos