STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Could any STMCU be used to drive dual LCD screens?

Hello Guys,I am searching for a MCU to drive dual LCD screens. Although I see some MCU (eg, STM32U5G9ZJTXQ) providing both DSI and RGB mode interfaces without pinout collision, I didn't see any description about whether the LTDC can output 2 differen...

srony by Associate II
  • 3665 Views
  • 7 replies
  • 3 kudos

Displaying 16bpp colour

Hi,We have recently upgraded a project from TouchGFX v4.10 to v4.24, and have a question about colour representation. We haven't been able to update the HAL- this is a legacy project and we don't have access to the .ioc file.We've replaced the deprec...

Emma__2-1742163521169.jpeg Emma__3-1742163526388.jpeg
Emma_ by Associate
  • 918 Views
  • 1 replies
  • 0 kudos

Custom Gauge with Button

Hi all,Can anyone please give me advice how can I implement a custom Gauge:That will be used my custom image and needle That can be also a button, that when I click in the middle of the gauge, the gauge will change image to glowing as it is a button ...

Resolved! Flawed vectorized font output (Designer 4.24.1)

Hi,I’d like to use the vectorized version of a font (bebas-neue-regular.ttf), but the glyphs don’t quite match the original shape. Why is that, and how can I fix it?Could it have something to do with the arrow next to some nodes? I don’t know much ab...

ferro_0-1741712284064.png ferro_1-1741712327180.png
ferro by Lead
  • 3001 Views
  • 7 replies
  • 2 kudos

Resolved! Error while renaming the touch gfx project

Hello All, I need to change the touch GFX project name MyApplication_747I to something else, I am trying to change it from config but touch gfx is not allowing it to change. I tried to edit and modify the  .touchgfx file and changed the name from "Na...

ShivDesh by Associate III
  • 1633 Views
  • 2 replies
  • 3 kudos