STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Scrolling text wider than the LCD screen

I am using TouchGFX Designer (version 4.24.1).I am wanting to stroll a Text Area across the screen. I can do this with the MoveAnimator selected as long as the text width is less than the screen width. When I attempt to scroll text than is wider than...

RWilt.1 by Associate II
  • 914 Views
  • 1 replies
  • 0 kudos

Resolved! TouchGFX 4.25.0 Flickering

Hello,I'm working with a graphics output on an STM32H750-based board.My bitmap resources are stored in SQPI, and the frame buffers (double buffering) are in external SDRAM.The external SDRAM settings are as follows: TEX=1, Bufferable=1, Cacheable=1, ...

nonoriri_0-1743052778716.png nonoriri_1-1743052802656.png
nonoriri by Associate III
  • 1665 Views
  • 2 replies
  • 2 kudos

TouchGFX Cygwin Error after rebasing

Hi, I'm using the STM32F769I-Eval board and have come accross the same Cygwin error which a lot of people seem to have come across. After reading through multiple posts the best solution I have found was here to use 'editbin' to perform the rebase as...

rriddell_0-1742907147877.png
rriddell by Associate II
  • 1597 Views
  • 4 replies
  • 2 kudos

Changing Colors of Vector Images

Hello,I understand there's been a similar question asked and answered here: https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/how-does-touchgfx-directly-change-the-color-of-the-picture-in/td-p/116908, but I'd really like to emphasize my desire ...

JAlbr.1 by Associate III
  • 1689 Views
  • 3 replies
  • 0 kudos

Resolved! Black screen with TouchGFX

I have just started using TouchGFX on an Stm32H7A3ZIQ Nucleo board. I managed to setup the LTDC correctly and am able to change the color of the screen, which makes me assume that the LTDC is setup correctly.After setting up TouchGFX with FreeRTOS, f...

DavidL__0-1742852938643.png DavidL__1-1742853015250.png DavidL__2-1742853056070.png DavidL__3-1742853200431.png
DavidL_ by Associate III
  • 1141 Views
  • 1 replies
  • 1 kudos

How to add X/Y line chart with multiple series

I have my own TouchGFX App running on STM32H747I-DISCO board. It reads data from popular BME280 sensor chip via I2C interface. Now I need to show the "history" of measured temperature, pressure and humidity on a graph underneath the RTC date, day of ...

Louie88 by Senior II
  • 1140 Views
  • 1 replies
  • 0 kudos