STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! CubeMX 5.5.0 + Touch GFX Designer 4.13: GUI can run without freeRTOS on own HW STM32F429\439 TFT RGB 16bit LTDC?

Hi, I have my own hardware that run without freeRTOS on STM32F429 with STemWin GUI.In the revision hw I'm evaluation to use UI based on Touch GFX latest ver 4.13 + CubeMX 5.5.0.Can I migrate my full application without use freeRTOS with Touch GFX UI?...

stm32l4R9 eval board demo firmware

Hello In my touchgfx project , I have to do some power consumption works. I know there is a demo firmware for stm32L4R9 evel board. I want to take a look at clock configurations and chrom art accelerator enabling/disabling functions but I cant find...

Epamuk by Associate III
  • 1417 Views
  • 3 replies
  • 0 kudos

Gauge Image only half appearing on screen, it simulates ok on ToughGFX designer and also with visual studio.

i have use example from TouchGFX Demo 1, ive gone through code but cant see anything obvious. with the 746 Disco board, above.i set up the project through TouchGFX designer, only one screen and copied code from example, here is the view.cpp i have c...

0690X00000D9vIlQAJ.jpg
BO Re.1 by Associate II
  • 2692 Views
  • 8 replies
  • 0 kudos

Resolved! Various screens vs various containers

Hello,If various elements of the GUI I'm working on are going to be shared amongst most of the screens (footer, header, status bar,…), do you think it's a good idea to use a single TouchGFX screen and to change only the central content by means of co...

GMeur by Senior II
  • 1077 Views
  • 1 replies
  • 0 kudos

Adding text while working

Hello!I work with textArea.I want to add new text while program working. For example - I get array of filenames and I want to put filenames to screen (and later select one of them by touching).How can I do this? How to create new textArea while pro...

EEuge by Senior
  • 1886 Views
  • 5 replies
  • 0 kudos

Resolved! TouchGFX violates global namespace standard

All declarations in the global namespace that start with an underscore are reserved by the C++ compiler according to the C++ standard. See: https://en.cppreference.com/w/cpp/keyword TouchGFX violates this by converting any images to "_filename" and ...

j o by Associate II
  • 1825 Views
  • 3 replies
  • 0 kudos

I am using a touchgfx scrollable container to create a list. I include a radio button in the container. My problem is: In the container the radio button is assigned to radioButtonGroup1.

When I select the radio button for a list element, the other list element radio buttons are not deselected. Is there a way to make the radiobuttongroup for all of the list elements the same?

MLync.1 by Associate II
  • 876 Views
  • 1 replies
  • 0 kudos

Transmit buffer generated by HAL_DCMI_Start_DMA over UART interface in Snapshot mode of low-resolution image

Can I transfer buffer generated HAL_DCMI_Start_DMA through UART interface. I am using STM32f4 discovery board. My UART stop working after HAL_DCMI_Start_DMA call. My main function is attached. int main(void){ /* USER CODE BEGIN 1 */ OV9655_IDTypeDef ...

Junaid by Associate II
  • 1085 Views
  • 1 replies
  • 0 kudos