2019-10-29 2:27 AM
I am using TouchGFX with STM32F767BI and 800x480 LCD.
I made a graph with reference to Graph during TouchGFX Demo.
My problem is that I can't set the Y axis.
How can I set it up?
The data I want to display is from 0 to 120000.
void Graph::setup(int newWidth, int newHeight, int bufSize, colortype lineColor, colortype backgroundColor)
{
setWidth(newWidth);
setHeight(newHeight);
graphLinePainter.setColor(lineColor);
graphAreaPainter.setColor(lineColor, getHeight());
graphDotsPainter.setColor(lineColor);
graphDotsBackgroundPainter.setColor(backgroundColor);
graphLine.setLinkedGraph(graphArea);
graphLine.setLinkedGraph(graphDots);
graphLine.setLinkedGraph(graphDotsBackground);
graphLine.setPosition(0, 0, getWidth(), getHeight());
graphLine.setPainter(graphLinePainter);
graphLine.setBuffer(graphBuffer, bufSize);
graphLine.setLineWidth(1);
graphLine.setRange(0, 290, 6500,0);
graphArea.setPainter(graphAreaPainter);
graphArea.setLineWidth(0);
graphDots.setPainter(graphDotsPainter);
graphDots.setLineWidth(7);
graphDots.setDotShape(0, 90);
graphDotsBackground.setPainter(graphDotsBackgroundPainter);
graphDotsBackground.setLineWidth(9);
graphDots.setDotShape(0, 30);
add(graphArea);
add(graphLine);
add(graphDotsBackground);
add(graphDots);
}This is almost the same Graph configuration as the example. I don't know how to change something.
2019-11-04 1:45 AM
Hi,
You specify the "range" of your values in the graphline.setRange() function.
/Martin
2019-11-04 4:26 AM
but it is not working.
2019-11-04 4:33 AM
Tell me what you mean by "not working" - The height of the graph will be the same, but the amount of values you can provide, the range, will be 0 to 120000.
/Martin
2019-11-04 3:29 PM
It is a problem when the following data is output from Demo Code.
int32_t slope_test[290] =
{
63,73,83,83,93,93,103,113,113,123,133,143,
153,173,183,193,213,233,243,263,283,313,333,363,
383,413,433,463,493,523,553,593,623,663,693,733,
783,833,883,933,993,1043,1103,1163,1223,1283,1343,1413,
1493,1573,1643,1723,1803,1883,1973,2053,2143,2233,2333,2433,
2533,2633,2743,2853,2963,3073,3193,3313,3433,3563,3693,3823,
3953,4083,4223,4363,4503,4643,4793,4943,5093,5243,5403,5553,
5723,5883,6043,6213,6383,6553,6723,6903,7083,7253,7433,7613,
7793,7973,8153,8343,8523,8703,8893,9073,9263,9453,9643,9823,
10013,10203,10393,10583,10773,10963,11153,11343,11523,11713,11893,12083,
12263,12443,12623,12803,12983,13153,13333,13503,13673,13843,14013,14183,
14353,14513,14673,14833,14993,15153,15303,15453,15603,15743,15883,16023,
16163,16303,16433,16563,16683,16813,16933,17053,17163,17283,17393,17503,
17613,17713,17813,17913,18013,18103,18193,18283,18363,18443,18523,18593,
18653,18723,18793,18853,18913,18973,19033,19093,19143,19203,19253,19303,
19343,19383,19423,19463,19503,19533,19573,19603,19633,19663,19693,19713,
19733,19753,19763,19783,19793,19813,19823,19833,19843,19843,19853,19853,
19863,19863,19863,19863,19863,19853,19853,19843,19833,19813,19803,19783,
19763,19743,19713,19693,19663,19633,19603,19573,19543,19503,19473,19433,
19393,19343,19293,19243,19193,19143,19083,19033,18973,18903,18843,18773,
18693,18623,18543,18463,18373,18293,18213,18123,18033,17943,17843,17753,
17653,17543,17443,17333,17223,17103,16983,16863,16743,16613,16483,16353,
16223,16083,15943,15803,15653,15513,15363,15213,15053,14903,14743,14583,
14423,14263,14093,13923,13753,13583,13403,13233,13053,12873,12693,12503,
12323,12133
};graphLine.setRange(-2, 216,120000,0);
The graph is printed but not normal.
2019-11-04 4:40 PM
like this.
2019-11-06 3:54 AM
Was it working with other ranges?
/Martin
2019-11-06 9:12 PM
hm....i tested max range 2000 it was good.