2019-10-25 2:09 AM
Hi,
I need to show "Yes/No" modal dialog when a sensor value goes over limits.
Why there is only Show/hide/move widget action, but no Action to show container? I'm I missing something here and thinking this wrong?
Should I make Custom Widget instead, or should I call C++ function that can show Container?
Thanks!
Solved! Go to Solution.
2019-11-06 2:31 AM
I can add a "Modal Window" to my canvas and select it as target after choosing the "Hide/Show widget" action.
A custom container or even a regular container is also a widget that you can select in the list of target widgets to show or hide,
/Martin
2019-10-25 9:16 AM
You can create a custom container of the "Yes/No" Modal Dialog and then add it inside your MainView after including the header file of the custom container.
Afterwards, you can set it visible or hide it in you custom code.
2019-10-28 6:53 AM
Okay, thanks!
So this feature could be added TouchGFX designer? I think this "show container" is commonly used feature, just like "show widget" is.
2019-10-31 6:37 AM
You're right, there are some inconsistensies when it comes to basic things like "show/hide".
/Martin
2019-11-06 2:31 AM
I can add a "Modal Window" to my canvas and select it as target after choosing the "Hide/Show widget" action.
A custom container or even a regular container is also a widget that you can select in the list of target widgets to show or hide,
/Martin