STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

RTC (Real Time Clock) and TouchGFX

EDIT:The main problem here is the initialization of the RTC clock.Is there known problems with initializing the RTC clock within a TouchGFX project?I'm having no luck with initializing the RTC in the context of TouchGFX.ORIGINAL POST:I'm working with...

TLahr.1 by Associate III
  • 2402 Views
  • 2 replies
  • 0 kudos

How to do it?

I have the OFF / ON button. I want one function in the system to be called when the button is pressed and another function is pressed. The button is set to TRIGGER / Toggle. How to do it?

AD�?b by Senior
  • 3172 Views
  • 8 replies
  • 0 kudos

Resolved! Zendesk vs ST website for TouchGFX support?

What is difference between being a member of st.com and touchgfx.zendesk.com?When I click community in Zendesk, I end up at st? Why should I not just log in to st?What does Zendesk give me that ST does not?

JOsen by Associate III
  • 1215 Views
  • 1 replies
  • 0 kudos

touchgfx with spi lcd

I arange the all settings acroding to information on https://touchgfx.zendesk.com/hc/en-us/articles/203642951-MCUs-without-TFT-controllerand when I try to debug my software on my custom board it says "can not execute Mi commands load ..."when I comme...

KERDO.1 by Associate II
  • 1875 Views
  • 5 replies
  • 0 kudos

Problem with interface with physical buttons

Hello!I try to create intefrace with physical buttons, following this instruction https://touchgfx.zendesk.com/hc/en-us/articles/205074551-Interfacing-with-physical-buttonsI Added  ../Middlewares/ST/touchgfx/framework/include/platform/driver/button...

EEuge by Senior
  • 3322 Views
  • 9 replies
  • 0 kudos

STM32F7 + USB HS +Touchgfx +FreeRTOS

Hello ST Team,I am working on USB HS HID Device only along with touchgfx +FreeRTOS in STM32F7 controller.But creates reading & writing Issue when touchgfx is included.I have even checked the clock but no use. 48Mhz is clock its proper.Any help would...

Uc.2361 by Associate II
  • 2625 Views
  • 5 replies
  • 0 kudos

Resolved! CubeMX 5.5.0 + Touch GFX Designer 4.13: GUI can run without freeRTOS on own HW STM32F429\439 TFT RGB 16bit LTDC?

Hi, I have my own hardware that run without freeRTOS on STM32F429 with STemWin GUI.In the revision hw I'm evaluation to use UI based on Touch GFX latest ver 4.13 + CubeMX 5.5.0.Can I migrate my full application without use freeRTOS with Touch GFX UI?...

stm32l4R9 eval board demo firmware

Hello In my touchgfx project , I have to do some power consumption works. I know there is a demo firmware for stm32L4R9 evel board. I want to take a look at clock configurations and chrom art accelerator enabling/disabling functions but I cant find...

Epamuk by Associate III
  • 1389 Views
  • 3 replies
  • 0 kudos

Gauge Image only half appearing on screen, it simulates ok on ToughGFX designer and also with visual studio.

i have use example from TouchGFX Demo 1, ive gone through code but cant see anything obvious. with the 746 Disco board, above.i set up the project through TouchGFX designer, only one screen and copied code from example, here is the view.cpp i have c...

0690X00000D9vIlQAJ.jpg
BO Re.1 by Associate II
  • 2646 Views
  • 8 replies
  • 0 kudos