cancel
Showing results for 
Search instead for 
Did you mean: 

Can I have multiple applications in a single master application?

Karan Kolhe
Associate III

I have one base application and have multiple applications and want to open close these multiple apps without closing a master application. All of them are created as an individual touchgfx project. Like in windows form application we open exe app using process.start and close exe app using this.close function . Is it possible to include all the projects created by different programmers in a single master app and then select any one of them

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Martin KJELDSEN
Chief III

I think you'd have to create a sort of boot loader that can jump to an address for a specific application. TouchGFX/Designer cannot help you accomplish that.

/Martin