STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to use internal flash as frame buffer?

I'm working a smart thermostat using STM32 and TouchGFX. So far I managed to implement major parts of my UI on a STM32F429-DISCO board. Now I'm trying to migrate to my custom board, which works differently from the discovery board mainly in 2 areas:1...

HAhan.1 by Associate II
  • 3611 Views
  • 5 replies
  • 0 kudos

Resolved! Switching Screen by HW button?

HI All,I'm having an issue regarding switching screen.in My GUI, i have Screen one and Screen two,1- in screen one i set an interaction for changing the current screen (to screen two) by hardware button and i generated the code correctly and i found ...

mibra.1 by Associate III
  • 3963 Views
  • 7 replies
  • 0 kudos

I would like to update clock on multiple screen where clock value i received from backend application Or from the model class

Hello @Martin KJELDSEN​ @Community member​ ,I have STM32F746G Disco Board.I have multiple screen in project and i would like to update the clock time on multiple screen.so, I have used the "digitalclock" widget at 3 different screen.I got the timing ...

Transistion to derived view class

HelloI have a View1, generated by the Designer and I can transision to this view.Now I want to create a View2, which View1 is it's base class and transistion to this View2.How can I do this?Thanks, Regards RS

RSchl.1 by Associate
  • 987 Views
  • 1 replies
  • 0 kudos