STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! texture mapper In the designer

Hello, everyoneWhen I adjusted the Angle in the designer, I got a lot of decimal places.why is this?I only use the buttons in the designer to adjust the Angle./korry

0693W000001prncQAA.png
Korry by Associate III
  • 1519 Views
  • 2 replies
  • 0 kudos

Resolved! I get an error just creating a new project

environmentTouchGFX4.12.3Select STM32F746G Discovery Kit in APPLICATION TEMPLATESelect Blank UI in UI TEMPLATE and createCreation of TouchGFX Application failed.Why?How can I check the error log?Thank you.

Ebun.1 by Senior
  • 1389 Views
  • 2 replies
  • 0 kudos

TouchGFX cacheing issue

Hi All,We are using STM32F429ZIT6 MCU with 8 Mega byte SD RAM connected to FMC peripheral. And 16 Mega Byte Serial flash which is connected via SPI. The internal memory is 2 MByte for this MCUWe are working on a touch GFX project wich have many asset...

Kpodu.1 by Associate II
  • 2072 Views
  • 3 replies
  • 0 kudos

ST778x library for small SPI TFTs

Good morning (o;Has someone came across a ST778x graphics library for controlling those small SPI TFTs?Seems the libs are only available for Arduino-like boards....Would also be interesting to know what the footprint of such a lib is if it exists...a...

Davorin by Senior
  • 1557 Views
  • 3 replies
  • 0 kudos