2018-09-26 3:56 AM
Hi,
I'm working on a project which needs to get the gesture of the user on the touchscreen.
Apparently the "BSP_TS_GetState(TS_StateTypeDef *TS_State)" function fills a structure of TS_StateTypeDef type.
typedef struct
{
uint8_t touchDetected;
uint16_t touchX[TS_MAX_NB_TOUCH];
uint16_t touchY[TS_MAX_NB_TOUCH];
#if (TS_MULTI_TOUCH_SUPPORTED == 1)
uint8_t touchWeight[TS_MAX_NB_TOUCH];
uint8_t touchEventId[TS_MAX_NB_TOUCH];
uint8_t touchArea[TS_MAX_NB_TOUCH];
uint32_t gestureId;
#endif
} TS_StateTypeDef;The TS_StateTypeDef contains the gestureId variable which takes the value of type @ref TS_GestureIdTypeDef. (GEST_ID_MOVE_UP, GEST_ID_MOVE_DOWN...)
typedef enum
{
GEST_ID_NO_GESTURE = 0x00, /*!< Gesture not defined / recognized */
GEST_ID_MOVE_UP = 0x01, /*!< Gesture Move Up */
GEST_ID_MOVE_RIGHT = 0x02, /*!< Gesture Move Right */
GEST_ID_MOVE_DOWN = 0x03, /*!< Gesture Move Down */
GEST_ID_MOVE_LEFT = 0x04, /*!< Gesture Move Left */
GEST_ID_ZOOM_IN = 0x05, /*!< Gesture Zoom In */
GEST_ID_ZOOM_OUT = 0x06, /*!< Gesture Zoom Out */
GEST_ID_NB_MAX = 0x07 /*!< max number of gesture id */
} TS_GestureIdTypeDef;So in my program i wrote :
//The full code is way more complicated, this part is just the problematic part
TS_StateTypeDef TS_Status; //My structure which will contain all the Touchscreen Datas
char buffer[50];//Text buffer
int main(void)
{
//Fill the TS_Status structure with the Touchscreen datas
BSP_TS_GetState(&TS_Status);
//Display on the LCD the TS_Status.gestureId Variable
sprintf(buffer, "%d", TS_Status.gestureId);
BSP_LCD_DisplayStringAt(0, LINE(0), &buffer, LEFT_MODE);
}The problem is that BSP_TS_GetState(&TS_Status) always returns TS_Status.gestureId at 0, even if i move my finger up, down, left...
I already tried with the BSP_TS_Get_GestureId(&TS_State) function, same problem...
Thank you for your help,
Mathieu.
2018-09-26 10:05 AM
Hi @BJAUM ,
Is only the gestureId which is wrong?
What do you get if you want to display touchX and touchY for example?
For the gestureId, you need to call ts_gesture_id_string_tab like what it is already done in STM32Cube_FW_F7_V1.12.0\Projects\STM32F769I-Discovery\Examples\BSP\Src\touchscreen.c:
/* Get updated gesture Id in global variable 'TS_State' */
ts_status = BSP_TS_Get_GestureId(&TS_State);
sprintf((char*)lcd_string, "Gesture Id = %s", ts_gesture_id_string_tab[TS_State.gestureId]);
BSP_LCD_SetTextColor(LCD_COLOR_WHITE);
BSP_LCD_DisplayStringAt(0, BSP_LCD_GetYSize() - 15, lcd_string, CENTER_MODE);Please try this way and let me know if this works for you.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-09-26 10:14 AM
I would like to add that ts_gesture_id_string_tab is declared in STM32Cube_FW_F7_V1.12.0\Drivers\BSP\STM32F769I-Discovery\stm32f769i_discovery_ts.c as following:
/* Table for touchscreen gesture Id information display on LCD : table indexed on enum @ref TS_GestureIdTypeDef information */
char * ts_gesture_id_string_tab[GEST_ID_NB_MAX] = { "None",
"Move Up",
"Move Right",
"Move Down",
"Move Left",
"Zoom In",
"Zoom Out"
};
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-09-26 1:27 PM
the firmware of the touch screen controller that st used, does not have gestures enabled
2020-03-01 11:21 PM
Hi,BJAUM:
Have you fixed this issue, I'm confused about the issue too.