STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

EU Language support

Hi,I'm wondering if TouchGFX supports all EU langauges?When checking the documentation about language (https://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-features/languages-and-characters/#list-of-supported-languages) I can'...

RGB Interface

Hey,i am planning to use an LCD With RGB 18 bit interface.In the LCD D.S there are only RGB+DE+DCLK Pins, without Hsync and Vsync.it works In DE mode without this pins.can the MCU work at this mode?Brpeleg

Pkats.1 by Associate II
  • 1961 Views
  • 2 replies
  • 0 kudos

Resolved! touchgfx vertical line noise..

I am working on a project to control LCD with a custom board using stm32f429IG.I succeeded in displaying the screen, but vertical line noise occurs in each element.It was confirmed that there was no abnormality in the arrangement data of each image u...

0693W000003P7jKQAS.jpg
ssooki by Associate III
  • 4770 Views
  • 8 replies
  • 0 kudos

how to scroll container scroll bar limit set?

I am creating my menu using ListLayout Example of TouchGFX example code.I want to set the Limit of the Scrollbar. But when I reviewed the current example and Class, I could not find that part.How can I set Limit ?????​The end of the current list is s...

0690X000008AQxAQAW.jpg 0690X000008AQxOQAW.jpg
ikassma by Senior
  • 4542 Views
  • 10 replies
  • 0 kudos

RTOS issue with STM32L4R9ZI new project

Hi,I have STM32L4R9 discovery board which uses STM32L4R9AI Ic and i am able to work on this using Touchgfx.We have our own developed PCB with STM32L4R9ZI IC. I used STMCubeMx software to generate project of STM32L4R9ZI. i saw the settings used in dev...

Bala1 by Associate II
  • 1653 Views
  • 2 replies
  • 0 kudos