STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Timestamp on X axis label

Hi,I'm currently working with the Dynamic Graph widget in TouchGFX, and I want to display X-axis labels in the format hh:mm:ss to show timestamps (e.g., 00:01:10, 00:01:20, etc.).Right now, the X-axis labels are just integers, in the range which corr...

Riya_L by Associate II
  • 438 Views
  • 1 replies
  • 0 kudos

Resolved! Issue with Vector Renderer and Memory Allocation

 Hello everyone,I am trying to use the Vector Renderer to draw lines because it utilizes GPU2D, which offers faster rendering compared to the Canvas. Below is the code I am using for this purpose: void TestWidget::draw(const touchgfx::Rect& invalidat...

TerZer by Associate III
  • 1275 Views
  • 3 replies
  • 0 kudos

Resolved! Broken images

Hi,I have a funny issue. I just wanted to add a Share button to my Main Screen in an STM32TouchGFX of a working Weather Station app but when I built and run the app in STMCubeIDE all the widgets which uses background images showed surprising garbage ...

20250415-img-extflash.png 20250415-TGFX-Config-Image-Group.png 20250415-img-intflash.png
Louie88 by Senior II
  • 4248 Views
  • 13 replies
  • 0 kudos

Resolved! DSI display is mirrored

I am working with a custom board I designed using this display(LINK) They provide init codes on the product page that I have integrated into my project but they do not provide any any porch, timing or polarity information.  I first setup LTDC and the...

1000000497.jpg Capture1.JPG 1000000496.jpg
brohr01 by Associate III
  • 6179 Views
  • 6 replies
  • 6 kudos

ST7796S SPI Display Driver

I'm wanting to connect a STM32F756 Nucleo board to a ST7796S-controlled 4" 320x480 TFT screen. Is there a good driver available for that? I can mostly find ones for ili9341.

jwade19 by Associate II
  • 6012 Views
  • 3 replies
  • 1 kudos