User Activity

Hello,I have integrated touch GFX with quad SPI, and images are stored in external flash, in debug mode the code is getting stuck inside the Hal Delay. What is the root cause for this, if I disable the external loader the Hal delay does not get stuck...
hello,I Have linked the Touch GFX folder from another project and the code got compiled while running and  Debug I am getting this error.
hello,In the Touch GFX application, I have integrated quad SPI, and I am getting the following error.Error: Data mismatch found at address 0x90000000 (byte = 0x00 instead of 0x89)  Error: Download verification failed 
Title edited to be more descriptive than just "USB"HI,I Need help, My application Requires  Firmware updates using USB DFU Mode, and planning to make a custom Pc software that updates code using USB. How can I Make sure that only my Pc software shoul...
HI,I have a Touch GFX-based application with External Quad SPI flash integrated for Assets, such as images and font. The Application code has more than 150 Screens Due to this internal flash is running out of memory, Even though we are using 0s optim...