Skip to main content
Visitor II
Feb 19, 2024 12:30 AM UTC
Solved

Unable to get LTDC working on STM32H735G-DK

Hello everyone

I recently bought an STM32H735G-DK Discovery Kit, which has a 480x272 parallel LCD. I got the TouchGFX Demo projects running on the board, so I know all the hardware is working as it should.

Eventually I want to use TouchGFX on a custom board, so I am trying to configure a new project 'from scratch'. I am very new to the STM32 ecosystem, so I thought I would keep things simple and try to display something on the LCD with a framebuffer in the internal RAM.

So I started a new project in the STM32CubeIDE, from an existing ioc file (the one from one of the TouchGFX examples). I then disabled OCTOSPI1, OCTOSPI2, FREERTOS, LIBJPEG, TOUCHGFX, CRC, in order to have a project which is as bare bones as possible.

Following this guide (https://support.touchgfx.com/docs/development/board-bring-up/how-to/02-cpu-running), i was able to access the internal RAM (with some trial and error, I found I could address bytes 0x08000000to 0x08100000.

I then continued to this guide (https://support.touchgfx.com/docs/development/board-bring-up/how-to/03-display-internal). I was able to see the LTDC interrupt working by utilizing break points in the debugger. I started with a partial framebuffer of 480x100. This way I am sure that it fits in the internal RAM.
However, I was not able to get a red screen, as I would expect following the tutorial. My screen stays black. I am unsure what I am doing wrong. I am also unsure what I should put in the 'Color Frame Buffer Start Address', since it seems I should declare the framebuffer myself? I feel like I am missing something, but I don't know what or where to look.

ltdc-config.png

 

I hope you can help me get past this 'issue'.

Kind regards

 

Anton

This topic has been closed for replies.
LouisBBest answer
ST Employee
May 30, 2025 9:19 AM UTC

Hello all,

The issue here is the ram that is, by default set in DTCM zone which cannot be read by the LTDC. More information here Solved: Unable to get LTDC to output contents of Frame Buf... - STMicroelectronics Community. In general, please avoid answering to an old thread and open a new one instead. 

 

BR,

Louis BOUDOST Software Engineer | TouchGFX

4 replies

Osman SOYKURT
ST Technical Moderator
Feb 26, 2024 5:00 PM UTC

Hello @hanton , 

I can see it's your first post in our forum. Welcome to the community :grinning_face:

It's an excellent idea to start with the board bring-up as you do. You'll for sure learn from it!

I briefly looked at your project and from the symptom you mentioned, I guess it could be due to some of the priority in here :

OsmanSOYKURT_1-1708966816616.png

 

The lower the number of the "Preemption priority" is, the higher is the priority.

If it's not this, you can try to run your program on your board, and use STM32CubeProgrammer to see it there's the data you expect in the memory range of your framebuffer. If there's no data, the HAL_LTDC_LineEventCallback() is probably never called.

ST Software Developer | TouchGFX
Osman SOYKURT
ST Technical Moderator
Mar 14, 2024 11:27 AM UTC

Hello @hanton 

Did you find a solution to your issue? Do you need more assistance?

ST Software Developer | TouchGFX
Nicholas Yunker_2
Senior
May 24, 2025 8:26 PM UTC

I seem to be having exactly the same problem...have you been able to fix the problem and if so, how did you do it?

LouisBBest answer
ST Employee
May 30, 2025 9:19 AM UTC

Hello all,

The issue here is the ram that is, by default set in DTCM zone which cannot be read by the LTDC. More information here Solved: Unable to get LTDC to output contents of Frame Buf... - STMicroelectronics Community. In general, please avoid answering to an old thread and open a new one instead. 

 

BR,

Louis BOUDOST Software Engineer | TouchGFX