Skip to main content
Associate III
Feb 24, 2025 8:40 AM UTC
Solved

how to use the 'button is clicked' to show or hide the image ?

how to use the 'button is clicked' to show or hide the image ? who can provide the sample program to be reference .

 

 

miker_0-1740386272525.png

 

    This topic has been closed for replies.
    GaetanGodart
    GaetanGodartBest answer
    ST Employee
    Feb 24, 2025 9:31 AM UTC

    Hello @miker ,

     

    You can use the method setVisible to manage the visibility of your image and you can use the isVisible method to know if it is currently visible or not.

    Please find attached an example where clicking on a button toggle the visibility of an image.
    Note that the code is directly inside the interaction as I do "execute C++ code" instead of "Call new virtual function".

     

    I hope this helps!
    If this post answers your question, I invite you to select it as "best answer".

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)

    5 replies

    GaetanGodart
    GaetanGodartBest answer
    ST Employee
    Feb 24, 2025 9:31 AM UTC

    Hello @miker ,

     

    You can use the method setVisible to manage the visibility of your image and you can use the isVisible method to know if it is currently visible or not.

    Please find attached an example where clicking on a button toggle the visibility of an image.
    Note that the code is directly inside the interaction as I do "execute C++ code" instead of "Call new virtual function".

     

    I hope this helps!
    If this post answers your question, I invite you to select it as "best answer".

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)
    mikerAuthor
    Associate III
    Feb 24, 2025 9:34 AM UTC

    miker_0-1740389561236.png

    whether use the 'hide widget' to execute this function ?if yes, could you have any sample program to be provided ?

    GaetanGodart
    ST Employee
    Feb 24, 2025 9:52 AM UTC

    The "Hide widget" action will only allow you to hide the image, not to set it back to visible.
    Also, it doesn't allow you to use a condition like I did with "!isVisible(image1)".

    So if you want to hide and unhide a widget with only interaction, you will need 2 buttons, one to hide the image and another one to show the widget.

    Please find an example attached.

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)
    mikerAuthor
    Associate III
    Feb 25, 2025 7:20 AM UTC

    i am a new comer for the TouchGFX, and now ,i want to click button '1' each time, then the image '2'/'3'/'4'/'5' can circularly be showed; so, when image '2/3/4/5' are overlapped together, the result is that small green circle is automatically increased and initial by press button '1'

     

     

    miker_0-1740467598576.png

     

    GaetanGodart
    ST Employee
    Feb 25, 2025 9:59 AM UTC

    Hello @miker ,

     

    Please, as Louis mentioned, only create a single thread per question.

    You stopped commenting on my answer in your previous thread .
    Did it help you?

    Let's continue the discussion on the previous post, I have merged both topics.

     

    Regards,

    Gaetan GodartSoftware engineer at ST (TouchGFX)