cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX KeyBoard samples.

ShivDesh
Associate III

Hello All Members,

I am building one project using STM32 controller and using TouchGFX for creation of GUI for touchpanel.

I am trying to look for the QWERTY keyboard, where I can be able to have LOGIN Screen and can provide option for User to select Characters, Numbers and Special Characters to set their username and Password.

It would be great if someone could provide me a direction, where I can get the Qwerty Keybord for my TouchGFX project.

Also please let me know how I can customize the keyboard if required ?

 

BR,

Shiv

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
urbito
Senior II

You should have a look on this post:

 

Share your Custom Widgets! - STMicroelectronics Community

 

there are couple of widgets and keyboards that may help you, also some examples on the TouchGFX app itself.

 

hope it helps.

 

Greetings

Osman SOYKURT
ST Employee

Hello @ShivDesh ,

I also recommend checking the Share your Custom Widgets! - STMicroelectronics Community thread as suggested by @urbito .

 

Have you been able to find what you need?

Osman SOYKURT
ST Software Developer | TouchGFX
Osman SOYKURT
ST Employee

Hello @ShivDesh ,

Did you find a solution to your issue?

Osman SOYKURT
ST Software Developer | TouchGFX

Hello @Osman SOYKURT ,

 

Not yet able to customize the Keyboard as needed but got one keyboard which I am using temporally for now.

It would be helpful to all Users if there is default inbuild Keyboard provided in touchgfx.

BR,

Shivprasad

Hello @ShivDesh ,

The easiest way would be to reuse and customize the custom container shared in here. I understand your need of having a native keyboard widget, this will be communicated to my team.

Osman SOYKURT
ST Software Developer | TouchGFX

Yes Sure Osman.

Thanks for sharing the information. If the Keyboard plan is changed in future to be more customizable, I might need play around it will keep you posted.

 

BR,
Shiv

Osman SOYKURT
ST Employee

You're welcome @ShivDesh ,

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question. Thanks :)

Osman SOYKURT
ST Software Developer | TouchGFX

Yes Osman,

Actually, I am still looking for a good solution.

If there is any document to do it or some direction you could provide that would be great.

What I need to follow to have a keyboard which can be customized. I mean having Enter space, char, num, special char, etc in it and changes to be done for it ?

If you could provide a source code and let me know the changes and steps to do it, that would be very helpful.

Thanks :) 

 

Hello @ShivDesh ,

I do not have other ideas than the ones that have been suggested already. 
If you need help to customize the Keyboard custom container, I recommend reaching out to our the ST Online Support Center. They can provide you with the necessary guidance, documentation, and source code to help you achieve your customization goals.

Osman SOYKURT
ST Software Developer | TouchGFX