STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! NUCLEO-F429/F439 RGB666 interface mapping

Hi,I need a development board with the rgb 666 interface to use a TFT display.Looking through the Nucleos, I found the NUCLEO-F429ZI and the NUCLEO-F439ZI which should include that interface.Reading the documentation of theese boards and their MCU, I...

CVill.2 by Associate
  • 2338 Views
  • 2 replies
  • 0 kudos

Resolved! "No Rule to make target" error

Project created in: TouchGFX Designer Board used: STM32F469I-Discovery BoardGenerated code in TouchGFX Designer TouchGFX Designer also creates STM32CubeIDE applicationReplaced the name in .project folder. "<name>STM32F469I-DISCO</name>" with my Proje...

Sayali by Associate II
  • 6862 Views
  • 4 replies
  • 0 kudos

Errors after generating code with TouchGFX Generator

Hello,I'm using the Mikromedia 7 Capacitive with the STM32F476ZG MCU. I'd like to make an application with TouchGFX. I followed the Generator User Guide but as soon as I tick Graphics Application from X-CUBE-TOUCHGFX, it generates two errors in app_t...

0693W00000D0am3QAB.png 0693W00000D0ammQAB.png
MLair.1 by Associate III
  • 1672 Views
  • 4 replies
  • 0 kudos

Resolved! Can we have a scrollbar on Scroll List Container?

Let say I define a 'Scroll List Container' in my Screen1 view. Inside the container I insert many items to the point they don't fit to the container view size. Is there anyway we can have scrollbar say on the right of the list and user can move up an...

BParh.1 by Senior III
  • 2301 Views
  • 5 replies
  • 0 kudos

Touchgfx and external flash with quadspi

Hi guys... I am trying to udpate an external flash during the booting process. We already developed an external loader which is working fine when we use it with stm32cube programmer. I developed a code for loading a file from a usb key and calling a ...

SGasp.1 by Senior
  • 1642 Views
  • 0 replies
  • 0 kudos

Resolved! change screen from Model.cpp

Hi I'd like to change screen from Model.cpp, regardless the screen I'm currently in.Is there a solution without implementing a method that changescreen in each screens ? Thanks !