STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX Designer fails to generate assets

Hello,I have installed the following on my Windows 10 PC:STM32CubeIDE v1.6.0STM32CubeMX v6.2.0 STM32CubeProgrammer v2.6.0TouchGFX v4.16.1From the CubeIDE I can compile and debug code on my STM32F469I-DISCO board.However if I try to create an example ...

HGray.1 by Associate II
  • 2107 Views
  • 3 replies
  • 1 kudos

Error to add a new Screen at touchgfx

Hello, I'm having a new problem with a touchGFX designer, when i try to add a new screen the CUBE IDE compiler generate many of erros.if i have 6 screens its okay, the CUBE IDE compile the code, but and i add the 7 screen, for some reason something h...

PCabr.1 by Associate II
  • 3366 Views
  • 0 replies
  • 0 kudos
DYann.1 by Senior II
  • 5756 Views
  • 19 replies
  • 1 kudos