cancel
Showing results for 
Search instead for 
Did you mean: 

I'm trying to use touchGFX 4.10.0 on a STM32F429I discovery. I'm a new user, so, apart the class refernce manual in STM32cube F4, is there any simple tutorial or getting started guide so I can understand how to move in this environment? Thanks

Hicss.2033
Associate III

Also some sample code, just to start, may be useful for unserstanding events and how to connect events to the microcontroller state.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
MM..1
Chief III

Examples is in designer start window and latest is 4.16.1

Alexandre RENOUX
Principal

Hello Hicsss.2033,

Like MM..1 mentioned, please use TouchGFX 4.16.1 with TouchGFX Designer. You will have many examples and demos.

Also I highly recommend you to read the documentation website.

When your question is answered, please close this topic by choosing Select as Best.

/Alexandre

I'm using system workbench and, for what I have inderstood, it works only with the version 4.10.0. Do the examples that you are citing work also for 4.10.0?

Thanks for your answer.

Where can I find the designer start windows? I'm using system workbench which, for what I undestood, is compatible only with 4.10.0.