User Activity

I've recently updated with no major issue my TouchGFX project from 4.18.1 to 4.20.0.The screen behaves like before with one major exception: all the slide transitions have become way slower and laggy now with the new version.When previously with 4.18...
Hello everyone,I'm currently developing a project using Touchgfx on a custom board with a STM32F469II and a 1024x600 screen on RGB565 format. I'm also using both an external SDRAM and Flash and the DMA2D is activated.Recently, I've been having an iss...
Hello everyone,I'm currently developing a project using Touchgfx on a custom board with a STM32F469II and a 1024x600 screen on RGB565 format. i'm using an external flash running at 100 MHz and an external SDRAM of 8 MB with 4 banks used like so:The f...
Hello,I'm currently trying to use the "X-CUBE-CLASSB" package I'v found there : X-CUBE-CLASSB - Class B 60730-1 and 60335-1 Functional Safety Package with software expansion for STM32Cube - STMicroelectronics to do some watchdog, stack and flash secu...
Hello,I'm currently developing a project using Touchgfx on a custom board with a STM32F469II, external RAM/FLASH, SD card and a 1024x600 screen.I've recently come across an issue when performing any animation (slide screen transition, scrollable cont...
Kudos from