STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Can I use QT Designer for stm32h7?

Hi, I wanted to know is it possible to use QT designer for GUI instead of TouchGFX.In TouchGFX, I can't use function "setGraphRangeX" for float values.And I wanted to switch to QT since I didn't find any solution for that. Any help would be appreciat...

ATavo.1 by Associate III
  • 2257 Views
  • 1 replies
  • 0 kudos

Does anyone know why you can't integrate a Touch-GFX project with STM32 Cube on the STM32F7508-DK board.

When I create the project on Touch-GFX and then import the project to the the STM32 Cube IDE , it build fine but when I run the program on the STM32F7508-D board it just becomes a white blank screen. When I click on the reset button it goes back to w...

PMold.1 by Associate III
  • 4466 Views
  • 7 replies
  • 1 kudos

Resolved! Create TouchGFX project with IAR Workbench

Hello everyone!I want to create a TouchGFX project using IAR Workbench. When creating the code with the STM32CubeMX software, I chose EWARM. But when I open the project with IAR workbench, in the workspace there is no gui and generated folder (I want...

TTú.1 by Associate III
  • 2424 Views
  • 3 replies
  • 0 kudos

How can I show a picture on a tft lcd?

Hi! I'm using stm32h750-custom board, and I want to show a picture on a 4.3 inch tft lcd with ltdc interface. I'm pretty sure that I adjusted ltdc setting correctly. I used image converter to convert the image (480*272pixels) and I add the exported h...

SHash.2 by Associate
  • 2039 Views
  • 3 replies
  • 0 kudos

How to use TouchGFX designer with STM32CubeMX

Hi,I'm new to stm32 and embedded programming in general. I am currently using the stm32l496ag discovery kit.I began by toying with the designer, using the ready-made configuration for my board.Now I'd like to delve deeper using the STM32CubeMX.Is it ...

CHech.1 by Associate III
  • 1070 Views
  • 1 replies
  • 0 kudos