STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

32F746GDISCOVERY TOUCH REPLACEMENT

Hi folks.Have broken with a hit the capacitive touch screen that covers the display. A big line has split the touch in two. One part is still responding the other one is dead.The board mounts an obscure LCD_Kunjian_ HT043C_40P_P080_FLEX_FOLDED accord...

SLa S.1 by Associate
  • 850 Views
  • 0 replies
  • 0 kudos

Resolved! QSPI SRAM as framebuffer and Parallel or MIPI DSI?

Hi,I have some questions regarding the implementation of an LCD with the STM32F479ii.The display we want to use, has a 800x480 resolution at 60Hz and can have either 16 or 24 bit color depth.A framebuffer for a display like that is of course not goin...

Resolved! Prototype on NUCLEO-F767ZI, but use STM32L4Rx for final build? Any considerations to keep in mind?

Hello kind community, I'm using the STM32 chip and the LTDC module as a dedicated TFT LCD display driver. Right now I am using the NUCLEO-F767ZI for prototyping, but would like to use an STM32L4R/Px chip for the final build. I don't anticipate it bei...

RMora.4 by Associate III
  • 1447 Views
  • 2 replies
  • 0 kudos

STM32F746 LTDC USAGE WITH LVDS DISPLAY

Hi,I have been using STM32F746 with TFT's of Medium Sizes up to 4.3" having RGB Interface on my custom boards. Now I want to Interface Large Display like 12.1" or 15". I know I need a RGB -LVDS Converter Chip , But I want to know How to use LTDC wit...

SMour.2 by Associate III
  • 2118 Views
  • 2 replies
  • 0 kudos