STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX proces bar bug.

Hi,I have problem with animations using touchgfx on STM32f429Do you know what could be the issue? https://youtu.be/1T9_9cQWMvoThanks for help :)

SKiel.1 by Associate II
  • 943 Views
  • 1 replies
  • 0 kudos

Resolved! I can't save images on external Flash Memory correctly

Hi, I have a custom board with STM32H7A3 using FMC, LLTC and other modules. I started to develop the firmware to change some images in a display. I made one project on TouchGFX with multiple images and fonts. I verify the BitmapDatabase.cpp and the a...

0693W00000KZdXTQA1.png 0693W00000KZddqQAD.png
LCris.1 by Associate II
  • 2863 Views
  • 9 replies
  • 0 kudos

Non-Graphic Slider

Because I am working on a project without external Flash, it is critical that use of images be highly restricted because of the impact on internal Flash usage. We'd like to use TGFX sliders, but it seems that the minimum footprint is about 30kB, an u...

DSwea.1 by Associate III
  • 1138 Views
  • 1 replies
  • 0 kudos

Long time support

Hello​are there any plans for supporting a specific TouchGFX version for many years like a LTS version?​​Best regard.​

TNeub.1 by Associate III
  • 1036 Views
  • 1 replies
  • 0 kudos

Resolved! MIPI-DSI Long Write Command error - Length sensitive

Hello everyone,Objective : Send pixel data to LCD module using DSI-HOST on APB command mode.What I can do :+ Read the LCD module's GRAM content ..+ Send basic commands like Turn ON / OFF the Display, Pixels, Sleep IN / OUT ..+ Send long write command...

AELGH1 by Associate II
  • 2386 Views
  • 1 replies
  • 0 kudos

Resolved! Hi, I'm using a STM32H757 MCU with a graphical display on my new board. I would like to insert on it a VNC server using TouchGFX tool; is it possible? Thanks.

I saw that with STemWIN library it was possible but is no longer supported on stm32h7 mcu and also in the ST page is reported to use toucgGFX (and stmCube) tools insted STemWIN.Hou can I add a VNC server module on TouchGFX?

Danix2k by Associate III
  • 2330 Views
  • 3 replies
  • 0 kudos