Skip to main content
MWetter
Associate III
January 14, 2022
Question

Problems with Scrollable Container and text

  • January 14, 2022
  • 4 replies
  • 1719 views

Hello everyone :)

I've got some problems with the Scrollable Container. I created a small application based on the "Scrollable Container example". If I scroll the text, there are some issues. There is a delay between scrolling and the updated display of the text. It does not run smoothly.

It does not matter if I enable scrolling vertical, horizontal or both.

But on the other screen is a (horizontal) Scroll List with 12 Icons. There is no problem.

It works perfectly. If anyone has a hint for me....

Thank you very much

This topic has been closed for replies.

4 replies

Romain DIELEMAN
ST Employee
January 14, 2022

Hi,

Could you provide more information or images on what issue you are facing with texts (maybe your project or code as well) ? What are you trying to do exactly ? How did you implement it ? What version of TouchGFX are you using ?

/Romain

MWetter
MWetterAuthor
Associate III
January 14, 2022

Oh sorry I forgot some things :)

Our evaluation board is the STM32H7B3-dk with a custom display (5", 800x480).

We use FreeRTOS, external SDRAM.

It works perfectly. There is just this one problem.

We used TouchGFX V4.15 with CubeMX 6.3 and CubeIDE1.5.1.

ktrofimo
Senior III
January 14, 2022

I had a weird issues with H7 too. It was memory performance issues, and finally they were solved with correct CM7 memory protection (caching and buffering). Check STM guidelines AN4861 "Creating a graphical application with LTDC" / section 4.6 Special recommendations for Cortex-M7 (STM32F7/H7) mentioned by @SofLit reply to my problem: https://community.st.com/s/question/0D73W000001N9NY/detail?s1oid=00Db0000000YtG6&s1nid=0DB0X000000DYbd&emkind=chatterCommentNotification&s1uid=0050X000007vlPS&emtm=1640338065814

MWetter
MWetterAuthor
Associate III
January 14, 2022

Thank you. I'll check it :)