STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! HardFault with TouchGFX ?

Hello,I have a project with custom stm32f769 oard and TouchGFX as GUI. I've done a lot of testing on simpler GUI (showing background and one button).I've also prepared additional task that will do communication with other boards.Everything seems to b...

bully by Senior
  • 10593 Views
  • 20 replies
  • 0 kudos

setDraggable() function

Hi,Why isn't there a function setDraggable() in the Drawable class, the same way there is a setTouchable() function ? (as of now, the setTouchable() serves too to prevent the dragEvents to be received by a given widget)I'm asking because many times, ...

GMeur by Senior II
  • 1585 Views
  • 3 replies
  • 0 kudos

How to do 800*480 LTDC Sync

I want to set it to LTDC and use the color keying function in STM32H7, but I had no choice but to use it custom mode.When I made the project with TGFX, it was custom setting.The strange thing is that the pixel width and height of LTDC and TGFX are di...

MKaan.1 by Associate
  • 1221 Views
  • 1 replies
  • 0 kudos

Re-configuring a STM32H747I-DISCO TouchGFX-generated project to use DSI-video mode instead of DSI-adapted command mode to write to the display

I am currently working on a project that will ultimately involve switching out the native display on the STM32H747I-DISCO with a new one (MDT0500AISC-MIPI). This new display utilizes a MIPI-DSI interface, but unlike the native display, does not have ...

AKlin.2 by Associate
  • 1943 Views
  • 2 replies
  • 0 kudos