STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Hello, I am looking for help in finding a problem with the LCD connected via the FMC interface. Some data sent is corrupted.

I have an LCD screen (ortustech COM20H2P74ULX) connected via FMC to the STM32L4 MCU and I have some communication problems as some of the data I write on the screen gets corrupted. I suspect a bad communication timing setup with the screen memory, bu...

0693W00000NpgLAQAZ.png 0693W00000NpgMwQAJ.png 0693W00000NpgMxQAJ.png 0693W00000NpgQ5QAJ.png
Dziadek by Associate
  • 804 Views
  • 0 replies
  • 0 kudos

The LCD is working but not showing any character?

Hi, I am using stm32f103 and IAR for codes.I am trying to use a character LCD 16x2 for my project. It turns on with 5 volt that I connect but not showing any character. I changed the potentiometer and still no sign of characters.I was wondering what ...

ATavo.1 by Associate III
  • 6946 Views
  • 6 replies
  • 0 kudos

Resolved! Wrong representation of screen. (Shifted image)

Sometimes an image tells more than a thousand words:As you can imagine, the dots shouldn't be shifted to the right as on my display (there is an offset on the x-axis)This is my very example template (lots of buttons to test my touch).I use the STM32F...

0693W00000LywVLQAZ.jpg
Jiimmy by Associate II
  • 2305 Views
  • 3 replies
  • 0 kudos

Import GUI project and modify resolution

To use a GUI from one project on another board, I tried to "Import GUI" through TouchGFX from a project developed on STM32G071 into another STM32F429I board and it works,The Import process on TouchGFX: Edit => Import GUI => BROWSE => exist project =>...

cvinc.11 by Associate
  • 1245 Views
  • 1 replies
  • 0 kudos

Dear Experts, I am new in using STM32H735-DK board. tried to download clock example in developement board. Download succeed but example not working. Two LEDS,LD1 & LD2 continues ON and display Blank. when i press RST button display just blink only.

STMicroelectronics ST-LINK GDB server. Version 5.9.1Copyright (c) 2021, STMicroelectronics. All rights reserved.Starting server with the following options:    Persistent Mode      : Disabled    Logging Level       : 1    Listen Port Number     : 6123...

Dharmesh by Associate II
  • 2220 Views
  • 3 replies
  • 0 kudos