STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX and CMake

Hello. I've been struggling to flash a simple TouchGFX application through the STM32 VS Code extension. I am using the Nucleo-G071RB dev board with the GFX01M2 display board. My project was initially created using the TouchGFX designer, then generate...

Screenshot 2025-06-10 152940.jpg
TS-LMG by Associate III
  • 2025 Views
  • 11 replies
  • 3 kudos

Resolved! Touch Not Working on STM32U5G9J-DK1

Hello, I am developing a Touch GUI for STM32U5G9J-DK1 using Touch GFX [ 4.25.0]+STM32CubeIDE [1.19.0]. The Display is working correctly, but touch input is not gettingdetected.  Following information will be helpful:  1. If any specific power/reset/i...

Trustzone & TouchGFX/GPU2D support

Hi!Trying to get a TouchGFX working with Trustzone has shown itself to be quite the hassle. Although I have worked through a lot of issues already, my latest one has deemed real stubborn.When enabling GPU2D in a trustzone enabled project, the code th...

Tobiasvb by Associate
  • 506 Views
  • 1 replies
  • 0 kudos

DSI Video Mode (RGB888) with ST7703 on STM32U5G9NJ

  uC – STM32U5G9NJH6Q Display – 720 × 720 (ST7703 panel) Display controller – ST7703 MIPI lanes – 2 lanes DSI Host Mode – Video Mode (DSI_VID_MODE_BURST) Pixel format – RGB888 Problem / Symptoms After the initial display setup (LP mode initia...

PAV by Associate
  • 529 Views
  • 0 replies
  • 0 kudos

Resolved! GPU2D NemaGFX on the STM32N6570-DK hangs

Hello,I'm trying to use the GPU2D on the STM32N6570-DK, with NemaGFX.However, the GPU hangs on random functions.Well actually every time the same funtions, but depending on the number of functions to be executed, so it seems it can only execute a lim...

Circle_unfinished_2.jpg RoundedRect_unfinished_2.jpg
Jack3 by Senior III
  • 1164 Views
  • 2 replies
  • 1 kudos